AXIS#.OBS.BW

Description

AXIS#.OBS.BW sets the frequency at which the observer starts being the dominant component in the velocity signal.


    • To maintain stability, the Observer bandwidth should not be set lower than 3x the velocity open loop bandwidth (where the open loop blue line crosses 0dB).
    • This setting cannot be changed while the amplifier is enabled in order to minimize unexpected disturbances.
  • The Observer is made up of a few components. Following is a block diagram of how the Observer is connected in the loops.

Versions

Action Version Notes
Implemented 02-04-03-000  

General Information

Type

Read/Write

Units

Hz

Range

1 to 8,000.000

Default Value

500

Data Type

Float
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
AXIS1.OBS.BW

5017h

01h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.OBS.BW

5117h

01h

Unsigned32

-

1000:1

Read/Write

No